FAQ Solenoid Valves
  Why does my solenoid valve not shut off / not shut off instantly / not open? Show summary
  Are Solenoid Valves affected by the Pressure Equipment Directive (PED)? Show summary
  Can Danfoss solenoid valves operate by themselves or do I need to buy other things? Show summary
  What valve do you recommend for de-mineralised or de-ionised or even sea water? Show summary
  What valves do you recommend for Vacum? Show summary
  When are calculations based on kv invalid? Show summary
  What happened to the code numbers for WRAS (WRc) approved solenoid valves? Show summary
  What kind of valve can I use for potable water? (WRAS approved) Show summary
  What is the significance of different power ratings of solenoid coils? Show summary
  Which kinds of media are your valves not suitable for? Show summary
  What is a kv-value? Show summary
  What is more important in selecting a valve size - system pressure / flow rate / port dimensions? Show summary
  What is the difference between direct and servo operation? Show summary
  Why does the coil on the valve seem to be very hot? Show summary
  Are Danfoss coils continuously rated? Show summary
  What if my system has back pressure? Show summary
  What IP ratings do the valves have? Show summary
  Which coil can I use on a valve? Show summary
  I have a coil here - which valve can I use? Show summary
  Can you supply coils for hazardous areas? Show summary
  Why do I have to order a valve and coil separately? Show summary